GATT Descriptor Property FlagsGATT Database#

Macros#


define | SL_BT_GATTDB_DESCRIPTOR_READ 0x1#

define | SL_BT_GATTDB_DESCRIPTOR_WRITE 0x2#

define | SL_BT_GATTDB_DESCRIPTOR_LOCAL_ONLY 0x200#

Detailed Description#

This enum defines the property flags for GATT characteristic descriptors.

Macro Definition Documentation#

◆ SL_BT_GATTDB_DESCRIPTOR_READ#

define SL_BT_GATTDB_DESCRIPTOR_READ 0x1#


A GATT client can read the descriptor value.

◆ SL_BT_GATTDB_DESCRIPTOR_WRITE#

define SL_BT_GATTDB_DESCRIPTOR_WRITE 0x2#


A GATT client can write the descriptor value.

◆ SL_BT_GATTDB_DESCRIPTOR_LOCAL_ONLY#

define SL_BT_GATTDB_DESCRIPTOR_LOCAL_ONLY 0x200#


The descriptor is local only and should be invisible to GATT clients.