sl_bt_evt_sm_bonding_failedSecurity Manager#
This event is triggered if the pairing or bonding procedure fails.
Data Structures#
struct | Data structure of the bonding_failed event. |
Macros#
# define | sl_bt_evt_sm_bonding_failed_id 0x040f00a0 Identifier of the bonding_failed event. |
Detailed Description#
This event is triggered if the pairing or bonding procedure fails.
Data Structure Documentation#
◆ sl_bt_evt_sm_bonding_failed_s#
struct sl_bt_evt_sm_bonding_failed_s#
Data structure of the bonding_failed event.
Data Fields
uint8_t | connection | Connection handle |
uint16_t | reason | Describes error that occurred |