sl_bt_evt_sm_passkey_displaySecurity Manager#

Indicates a request to display the passkey to the user.

Data Structures#


struct | sl_bt_evt_sm_passkey_display_s | Data structure of the passkey_display event.

Macros#


define | sl_bt_evt_sm_passkey_display_id 0x000f00a0#

| Identifier of the passkey_display event.

Detailed Description#

Indicates a request to display the passkey to the user.


Data Structure Documentation#

◆ sl_bt_evt_sm_passkey_display_s#

struct sl_bt_evt_sm_passkey_display_s#

Data structure of the passkey_display event.

Data Fields#

uint8_t | connection |

Connection handle

uint32_t | passkey |

Passkey. Range: 0 to 999999.

  • NOTE! When displaying the passkey to the user, prefix the number with zeros to obtain a 6 digit number

  • Example: Passkey value is 42

  • Number to display to the user is 000042