sl_bt_evt_dfu_bootDevice Firmware Update#

This event indicates that the device booted in DFU mode and is now ready to receive commands related to device firmware upgrade (DFU).

Data Structures#

struct

sl_bt_evt_dfu_boot_s

Data structure of the boot event.

Macros#

# define

sl_bt_evt_dfu_boot_id 0x000000a0

Identifier of the boot event.

Detailed Description#

This event indicates that the device booted in DFU mode and is now ready to receive commands related to device firmware upgrade (DFU).


Data Structure Documentation#

◆ sl_bt_evt_dfu_boot_s#

struct sl_bt_evt_dfu_boot_s#

Data structure of the boot event.

Data Fields

uint32_t

version

The version of the bootloader