sl_bt_evt_dfu_bootDevice Firmware Update#
This event indicates that the device booted in DFU mode and is now ready to receive commands related to device firmware upgrade (DFU).
Data Structures#
struct | Data structure of the boot event. |
Macros#
#define | sl_bt_evt_dfu_boot_id 0x000000a0 Identifier of the boot event. |
Detailed Description#
This event indicates that the device booted in DFU mode and is now ready to receive commands related to device firmware upgrade (DFU).
Data Structure Documentation#
◆ sl_bt_evt_dfu_boot_s#
struct sl_bt_evt_dfu_boot_s#
Data structure of the boot event.
Data Fields#
uint32_t | version |
The version of the bootloader