sl_bt_evt_connection_parametersConnection#
Triggered whenever the connection parameters are changed and at any time a connection is established.
Data Structures#
struct | sl_bt_evt_connection_parameters_s Data structure of the parameters event. |
Macros#
#define | sl_bt_evt_connection_parameters_id 0x020600a0 Identifier of the parameters event. |
Detailed Description#
Triggered whenever the connection parameters are changed and at any time a connection is established.
Data Structure Documentation#
◆ sl_bt_evt_connection_parameters_s#
struct sl_bt_evt_connection_parameters_s#
Data structure of the parameters event.
Data Fields#
uint8_t | connection |
Connection handle
uint16_t | interval |
Connection interval. Time = Value x 1.25 ms
uint16_t | latency |
Peripheral latency (how many connection intervals the peripheral can skip)
uint16_t | timeout |
Supervision timeout. Time = Value x 10 ms
uint8_t | security_mode |
Enum sl_bt_connection_security_t. Connection security mode. Values:
sl_bt_connection_mode1_level1 (0x0): No security
sl_bt_connection_mode1_level2 (0x1): Unauthenticated pairing with encryption
sl_bt_connection_mode1_level3 (0x2): Authenticated pairing with encryption
sl_bt_connection_mode1_level4 (0x3): Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key
uint16_t | txsize |
Maximum Data Channel PDU Payload size that the controller can send in an air packet