sl_bt_evt_system_external_signalSystem#
Indicates that the external signals have been received.
Data Structures#
struct | sl_bt_evt_system_external_signal_s Data structure of the external_signal event. |
Macros#
#define | sl_bt_evt_system_external_signal_id 0x030100a0 Identifier of the external_signal event. |
Detailed Description#
Indicates that the external signals have been received.
External signals are generated from the native application.
Data Structure Documentation#
◆ sl_bt_evt_system_external_signal_s#
struct sl_bt_evt_system_external_signal_s#
Data structure of the external_signal event.
Data Fields#
uint32_t | extsignals |
Bitmask of external signals received since last event.