sl_bt_evt_system_bootSystem#
Indicates that the device has started and the radio is ready.
Data Structures#
struct | Data structure of the boot event. |
Macros#
#define | sl_bt_evt_system_boot_id 0x000100a0 Identifier of the boot event. |
Detailed Description#
Indicates that the device has started and the radio is ready.
This event carries the firmware build number and other software and hardware identification codes.
Data Structure Documentation#
◆ sl_bt_evt_system_boot_s#
struct sl_bt_evt_system_boot_s#
Data structure of the boot event.
Data Fields#
uint16_t | major |
Major release version
uint16_t | minor |
Minor release version
uint16_t | patch |
Patch release number
uint16_t | build |
Build number
uint32_t | bootloader |
Bootloader version
uint16_t | hw |
Hardware type
uint32_t | hash |
Version hash