sl_bt_evt_system_errorSystem#
Indicates that an error has occurred.
Data Structures#
struct | Data structure of the error event. |
Macros#
#define | sl_bt_evt_system_error_id 0x060100a0 Identifier of the error event. |
Detailed Description#
Indicates that an error has occurred.
See error codes table for more information.
Data Structure Documentation#
◆ sl_bt_evt_system_error_s#
struct sl_bt_evt_system_error_s#
Data structure of the error event.
Data Fields#
uint16_t | reason |
Result code
0: success
Non-zero: an error has occurred
uint8array | data |
Data related to the error; this field can be empty.