sl_bt_evt_system_hardware_errorSystem#
Indicates that a hardware-related error has occurred.
Data Structures#
struct | sl_bt_evt_system_hardware_error_s Data structure of the hardware_error event. |
Macros#
#define | sl_bt_evt_system_hardware_error_id 0x050100a0 Identifier of the hardware_error event. |
Detailed Description#
Indicates that a hardware-related error has occurred.
Data Structure Documentation#
◆ sl_bt_evt_system_hardware_error_s#
struct sl_bt_evt_system_hardware_error_s#
Data structure of the hardware_error event.
Data Fields#
uint16_t | status |
Result code
0: success
Non-zero: an error has occurred