sl_bt_evt_system_hardware_errorSystem#

Indicates that a hardware-related error has occurred.

Data Structures#


struct | sl_bt_evt_system_hardware_error_s | Data structure of the hardware_error event.

Macros#


define | sl_bt_evt_system_hardware_error_id 0x050100a0#

| Identifier of the hardware_error event.

Detailed Description#

Indicates that a hardware-related error has occurred.


Data Structure Documentation#

◆ sl_bt_evt_system_hardware_error_s#

struct sl_bt_evt_system_hardware_error_s#

Data structure of the hardware_error event.

Data Fields#

uint16_t | status |

Result code

  • 0: success

  • Non-zero: an error has occurred