sl_bt_evt_system_bootSystem#

Indicates that the device has started and the radio is ready.

Data Structures#


struct | [sl_bt_evt_system_boot_s](/bluetooth/<docspace-docleaf-version>/bluetooth-data-structures/group-sl-bt-evt-system-boot#structsl-bt- evt-system-boot-s) | Data structure of the boot event.

Macros#


define | sl_bt_evt_system_boot_id 0x000100a0#

| Identifier of the boot event.

Detailed Description#

Indicates that the device has started and the radio is ready.

This event carries the firmware build number and other software and hardware identification codes.


Data Structure Documentation#

◆ sl_bt_evt_system_boot_s#

struct sl_bt_evt_system_boot_s#

Data structure of the boot event.

Data Fields#

uint16_t | major |

Major release version

uint16_t | minor |

Minor release version

uint16_t | patch |

Patch release number

uint16_t | build |

Build number

uint32_t | bootloader |

Bootloader version

uint16_t | hw |

Hardware type

uint32_t | hash |

Version hash