sl_bt_evt_system_errorSystem#

Indicates that an error has occurred.

Data Structures#


struct | [sl_bt_evt_system_error_s](/bluetooth/<docspace-docleaf-version>/bluetooth-commnd-events-system/group-sl-bt-evt-system-error#structsl- bt-evt-system-error-s) | Data structure of the error event.

Macros#


define | sl_bt_evt_system_error_id 0x060100a0#

| Identifier of the error event.

Detailed Description#

Indicates that an error has occurred.

See error codes table for more information.


Data Structure Documentation#

◆ sl_bt_evt_system_error_s#

struct sl_bt_evt_system_error_s#

Data structure of the error event.

Data Fields#

uint16_t | reason |

Result code

  • 0: success

  • Non-zero: an error has occurred

uint8array | data |

Data related to the error; this field can be empty.