sl_bt_evt_system_soft_timerSystem#

Indicates that a soft timer has lapsed.

Data Structures#


struct | sl_bt_evt_system_soft_timer_s | Data structure of the soft_timer event.

Macros#


define | sl_bt_evt_system_soft_timer_id 0x070100a0#

| Identifier of the soft_timer event.

Detailed Description#

Indicates that a soft timer has lapsed.


Data Structure Documentation#

◆ sl_bt_evt_system_soft_timer_s#

struct sl_bt_evt_system_soft_timer_s#

Data structure of the soft_timer event.

Data Fields#

uint8_t | handle |

Timer Handle