sl_bt_evt_system_external_signalSystem#

Indicates that the external signals have been received.

Data Structures#


struct | sl_bt_evt_system_external_signal_s | Data structure of the external_signal event.

Macros#


define | sl_bt_evt_system_external_signal_id 0x030100a0#

| Identifier of the external_signal event.

Detailed Description#

Indicates that the external signals have been received.

External signals are generated from the native application.


Data Structure Documentation#

◆ sl_bt_evt_system_external_signal_s#

struct sl_bt_evt_system_external_signal_s#

Data structure of the external_signal event.

Data Fields#

uint32_t | extsignals |

Bitmask of external signals received since last event.