sl_bt_evt_connection_tx_powerConnection#
Reports a transmit power change on the local device of a connection if transmit power reporting has been enabled.
Data Structures#
struct | sl_bt_evt_connection_tx_power_s Data structure of the tx_power event. |
Macros#
#define | sl_bt_evt_connection_tx_power_id 0x060600a0 Identifier of the tx_power event. |
Detailed Description#
Reports a transmit power change on the local device of a connection if transmit power reporting has been enabled.
Enable or disable transmit power reporting using sl_bt_connection_set_power_reporting command.
Data Structure Documentation#
◆ sl_bt_evt_connection_tx_power_s#
struct sl_bt_evt_connection_tx_power_s#
Data structure of the tx_power event.
Data Fields#
uint8_t | connection |
Handle of the connection
uint8_t | phy |
Enum sl_bt_gap_phy_coding_t. The PHY which the transmit power is reported for. Values:
sl_bt_gap_phy_coding_1m_uncoded (0x1): 1M PHY
sl_bt_gap_phy_coding_2m_uncoded (0x2): 2M PHY
sl_bt_gap_phy_coding_125k_coded (0x4): 125k Coded PHY (S=8)
sl_bt_gap_phy_coding_500k_coded (0x8): 500k Coded PHY (S=2)
int8_t | power_level |
Transmit power level. Values:
Range -127 to 20: The transmit power level in dBm
SL_BT_CONNECTION_TX_POWER_UNAVAILABLE (0x7F): Transmit power level is not available.
uint8_t | flags |
Enum sl_bt_connection_tx_power_flag_t. Transmit power level flags.
Ignore this field if power_level is set to 0x7E or 0x7F. Values:
sl_bt_connection_tx_power_at_minimum (0x1): Transmit power level is at minimum level.
sl_bt_connection_tx_power_at_maximum (0x2): Transmit power level is at maximum level.
int8_t | delta |
Change in transmit power level. Values:
SL_BT_CONNECTION_TX_POWER_CHANGE_UNAVAILABLE (0x7F): Change is not available or is out of range.
Other values: positive indicates increased power, negative indicates decreased power, and zero indicates unchanged. Units: dB