sl_bt_evt_gatt_procedure_completedGATT Client#
Indicates that the current GATT procedure was completed successfully or that it failed with an error.
Data Structures#
struct | sl_bt_evt_gatt_procedure_completed_s Data structure of the procedure_completed event. |
Macros#
#define | sl_bt_evt_gatt_procedure_completed_id 0x060900a0 Identifier of the procedure_completed event. |
Detailed Description#
Indicates that the current GATT procedure was completed successfully or that it failed with an error.
All GATT commands excluding sl_bt_gatt_write_characteristic_value_without_response and sl_bt_gatt_send_characteristic_confirmation will trigger this event. As a result, the application must wait for this event before issuing another GATT command (excluding the two aforementioned exceptions).
Note: After a failed GATT procedure with SL_STATUS_TIMEOUT error, further GATT transactions over this connection are not allowed by the stack.
Data Structure Documentation#
◆ sl_bt_evt_gatt_procedure_completed_s#
struct sl_bt_evt_gatt_procedure_completed_s#
Data structure of the procedure_completed event.
Data Fields#
uint8_t | connection |
Connection handle
uint16_t | result |
Result code
0: success
Non-zero: an error has occurred