sl_bt_evt_sm_list_bonding_entrySecurity Manager#
Triggered by the command sl_bt_sm_list_all_bondings if bondings exist in the local database.
Data Structures#
struct | sl_bt_evt_sm_list_bonding_entry_s Identifier of the list_bonding_entry event. |
Macros#
#define | sl_bt_evt_sm_list_bonding_entry_id 0x050f00a0 Identifier of the list_bonding_entry event. |
Detailed Description#
Triggered by the command sl_bt_sm_list_all_bondings if bondings exist in the local database.
Data Structure Documentation#
◆ sl_bt_evt_sm_list_bonding_entry_s#
struct sl_bt_evt_sm_list_bonding_entry_s#
Data structure of the list_bonding_entry event.
Data Fields#
uint8_t | bonding |
Bonding handle
bd_addr | address |
Bluetooth address of the remote device
uint8_t | address_type |
Enum sl_bt_gap_address_type_t. Address type. Values:
sl_bt_gap_public_address (0x0): Public device address
sl_bt_gap_static_address (0x1): Static device address