sl_bt_evt_advertiser_scan_requestAdvertiser#
Reports any scan request received in advertising mode if the scan request notification is enabled.
Data Structures#
struct | sl_bt_evt_advertiser_scan_request_s Data structure of the scan_request event. |
Macros#
#define | sl_bt_evt_advertiser_scan_request_id 0x020400a0 Identifier of the scan_request event. |
Detailed Description#
Reports any scan request received in advertising mode if the scan request notification is enabled.
Do not confuse this event with the scan response.
Data Structure Documentation#
◆ sl_bt_evt_advertiser_scan_request_s#
struct sl_bt_evt_advertiser_scan_request_s#
Data structure of the scan_request event.
Data Fields#
uint8_t | handle |
Advertising set handle where scan request was received
bd_addr | address |
Bluetooth address of the scanning device
uint8_t | address_type |
Scanner address type. Values:
0: Public address
1: Random address
uint8_t | bonding |
Bonding handle if the remote scanning device has previously bonded with the local device. Values:
SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding
Other: Bonding handle