sl_bt_evt_gatt_characteristicGATT Client#

Indicates that a GATT characteristic in the remote GATT database was discovered.

Data Structures#

struct

sl_bt_evt_gatt_characteristic_s

Data structure of the characteristic event.

Macros#

#define

sl_bt_evt_gatt_characteristic_id 0x020900a0

Identifier of the characteristic event.

Detailed Description#

Indicates that a GATT characteristic in the remote GATT database was discovered.

This event is generated after issuing either the sl_bt_gatt_discover_characteristics or sl_bt_gatt_discover_characteristics_by_uuid command.


Data Structure Documentation#

◆ sl_bt_evt_gatt_characteristic_s#

struct sl_bt_evt_gatt_characteristic_s#

Data structure of the characteristic event.

Data Fields#

uint8_t | connection |

Connection handle

uint16_t | characteristic |

GATT characteristic handle

uint8_t | properties |

Characteristic properties

uint8array | uuid |

Characteristic UUID in little endian format