sl_bt_evt_sm_bondedSecurity Manager#
Triggered after the pairing or bonding procedure is successfully completed.
Data Structures#
struct | Data structure of the bonded event. |
Macros#
#define | sl_bt_evt_sm_bonded_id 0x030f00a0 Identifier of the bonded event. |
Detailed Description#
Triggered after the pairing or bonding procedure is successfully completed.
Data Structure Documentation#
◆ sl_bt_evt_sm_bonded_s#
struct sl_bt_evt_sm_bonded_s#
Data structure of the bonded event.
Data Fields#
uint8_t | connection |
Connection handle
uint8_t | bonding |
Bonding handle. Values:
SL_BT_INVALID_BONDING_HANDLE (0xff): Pairing completed without bonding - the pairing key will be discarded after disconnection.
Other: Procedure completed, pairing key stored with given bonding handle
uint8_t | security_mode |
Enum sl_bt_connection_security_t. Connection security mode. Values:
sl_bt_connection_mode1_level2 (0x1): Unauthenticated pairing with encryption
sl_bt_connection_mode1_level3 (0x2): Authenticated pairing with encryption
sl_bt_connection_mode1_level4 (0x3): Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key