sl_bt_evt_sm_confirm_passkeySecurity Manager#
Indicates a request for passkey display and confirmation by the user.
Data Structures#
struct | sl_bt_evt_sm_confirm_passkey_s Data structure of the confirm_passkey event. |
Macros#
#define | sl_bt_evt_sm_confirm_passkey_id 0x020f00a0 Identifier of the confirm_passkey event. |
Detailed Description#
Indicates a request for passkey display and confirmation by the user.
Use the command sl_bt_sm_passkey_confirm to accept or reject the displayed passkey.
Data Structure Documentation#
◆ sl_bt_evt_sm_confirm_passkey_s#
struct sl_bt_evt_sm_confirm_passkey_s#
Data structure of the confirm_passkey event.
Data Fields#
uint8_t | connection |
Connection handle
uint32_t | passkey |
Passkey. Range: 0 to 999999.
NOTE! When displaying the passkey to the user, prefix the number with zeros to obtain a 6 digit number
Example: Passkey value is 42
Number to display to the user is 000042