sl_bt_evt_connection_rssiConnection#
Triggered when an connection_get_rssi command has completed.
Data Structures#
struct | Data structure of the rssi event. |
Macros#
#define | sl_bt_evt_connection_rssi_id 0x030600a0 Identifier of the rssi event. |
Detailed Description#
Triggered when an connection_get_rssi command has completed.
Data Structure Documentation#
◆ sl_bt_evt_connection_rssi_s#
struct sl_bt_evt_connection_rssi_s#
Data structure of the rssi event.
Data Fields#
uint8_t | connection |
Connection handle
uint8_t | status |
Command complete status:
0x00: The command succeeded
0x01-0xFF: The command failed. See Bluetooth Core specification v5.0 [Vol 2] Part D, Error Codes
int8_t | rssi |
The median of the last seven measured RSSI values on the connection. Units: dBm. Range: -127 to +20. Ignore this parameter if the command fails.