sl_bt_evt_sm_confirm_bondingSecurity Manager#

Indicates a user request to display that the new bonding request is received and for the user to confirm the request.

Data Structures#

struct

sl_bt_evt_sm_confirm_bonding_s

Data structure of the confirm_bonding event.

Macros#

#define

sl_bt_evt_sm_confirm_bonding_id 0x090f00a0

Identifier of the confirm_bonding event.

Detailed Description#

Indicates a user request to display that the new bonding request is received and for the user to confirm the request.

Use the command sl_bt_sm_bonding_confirm to accept or reject the bonding request.


Data Structure Documentation#

◆ sl_bt_evt_sm_confirm_bonding_s#

struct sl_bt_evt_sm_confirm_bonding_s#

Data structure of the confirm_bonding event.

Data Fields#

uint8_t | connection |

Connection handle

uint8_t | bonding_handle |

Bonding handle for the request. Range: 0 to 31, or SL_BT_INVALID_BONDING_HANDLE (0xff).

  • NOTE! When the bonding handle is anything other than SL_BT_INVALID_BONDING_HANDLE (0xff), a bonding already exists for this connection. Overwriting the existing bonding is a potential security risk.