sl_bt_evt_gatt_server_user_read_requestGATT Server#
Indicates that a remote GATT client is attempting to read a value of an attribute from the local GATT database, where the attribute was defined in the GATT database XML file to have the type="user".
Data Structures#
struct | sl_bt_evt_gatt_server_user_read_request_s Data structure of the user_read_request event. |
Macros#
#define | sl_bt_evt_gatt_server_user_read_request_id 0x010a00a0 Identifier of the user_read_request event. |
Detailed Description#
Indicates that a remote GATT client is attempting to read a value of an attribute from the local GATT database, where the attribute was defined in the GATT database XML file to have the type="user".
The parameter att_opcode informs which GATT procedure was used to read the
value. The application needs to respond to this request by using the
sl_bt_gatt_server_send_user_read_response command within 30 seconds,
otherwise further GATT transactions are not allowed by the remote side.
Data Structure Documentation#
◆ sl_bt_evt_gatt_server_user_read_request_s#
struct sl_bt_evt_gatt_server_user_read_request_s#
Data structure of the user_read_request event.
Data Fields#
uint8_t | connection |
Connection handle
uint16_t | characteristic |
GATT characteristic handle. This value is normally received from the gatt_characteristic event.
uint8_t | att_opcode |
Enum sl_bt_gatt_att_opcode_t. Attribute opcode that informs the procedure from which the value was received.
uint16_t | offset |
Value offset