sl_bt_evt_sm_bondedSecurity Manager#

Triggered after the pairing or bonding procedure is successfully completed.

Data Structures

struct  

sl_bt_evt_sm_bonded_s

Data structure of the bonded event.

Macros

#define  

sl_bt_evt_sm_bonded_id   0x030f00a0

Identifier of the bonded event.

Detailed Description#

Triggered after the pairing or bonding procedure is successfully completed.


Data Structure Documentation#

◆sl_bt_evt_sm_bonded_s#

struct sl_bt_evt_sm_bonded_s

Data structure of the bonded event.

Data Fields

name

description

uint8_t

connection

Connection handle

uint8_t

bonding

Bonding handle. Values:

  • SL_BT_INVALID_BONDING_HANDLE (0xff): Pairing completed without bonding - the pairing key will be discarded after disconnection.

  • Other: Procedure completed, pairing key stored with given bonding handle

uint8_t

security_mode

Connection security mode. Values:

  • sl_bt_connection_mode1_level2 (0x1): Unauthenticated pairing with encryption

  • sl_bt_connection_mode1_level3 (0x2): Authenticated pairing with encryption

  • sl_bt_connection_mode1_level4 (0x3): Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key