sl_bt_evt_sm_bonding_failedSecurity Manager#

This event is triggered if the pairing or bonding procedure fails.

Data Structures

struct  

sl_bt_evt_sm_bonding_failed_s

Data structure of the bonding_failed event.

Macros

#define  

sl_bt_evt_sm_bonding_failed_id   0x040f00a0

Identifier of the bonding_failed event.

Detailed Description#

This event is triggered if the pairing or bonding procedure fails.


Data Structure Documentation#

◆sl_bt_evt_sm_bonding_failed_s#

struct sl_bt_evt_sm_bonding_failed_s

Data structure of the bonding_failed event.

Data Fields

name

description

uint8_t

connection

Connection handle

uint16_t

reason

Describes error that occurred