sl_bt_evt_sm_passkey_displaySecurity Manager#

Indicates a request to display the passkey to the user.

Data Structures

struct  

sl_bt_evt_sm_passkey_display_s

Data structure of the passkey_display event.

Macros

#define  

sl_bt_evt_sm_passkey_display_id   0x000f00a0

Identifier of the passkey_display event.

Detailed Description#

Indicates a request to display the passkey to the user.


Data Structure Documentation#

◆sl_bt_evt_sm_passkey_display_s#

struct sl_bt_evt_sm_passkey_display_s

Data structure of the passkey_display event.

Data Fields

name

description

uint8_t

connection

Connection handle

uint32_t

passkey

Passkey. Range: 0 to 999999. NOTE! When displaying the passkey to the user, prefix the number with zeros to obtain a 6 digit number

  • Example: Passkey value is 42

  • Number to display to the user is 000042