Advertising and Scan Response data struct, Core v5.3, Vol 3, Part C, S. 11.

Public Attributes#

uint8_t
uint8_t
sl_bt_ead_randomizer_t *
uint8_t *
sl_bt_ead_mic_t *

Public Attribute Documentation#

length#

uint8_t sl_bt_ead_ad_structure_s::length

Definition at line 81 of file common/ead_core/sl_bt_ead_core.h

ad_type#

uint8_t sl_bt_ead_ad_structure_s::ad_type

Definition at line 82 of file common/ead_core/sl_bt_ead_core.h

randomizer#

sl_bt_ead_randomizer_t* sl_bt_ead_ad_structure_s::randomizer

Definition at line 83 of file common/ead_core/sl_bt_ead_core.h

ad_data#

uint8_t* sl_bt_ead_ad_structure_s::ad_data

Definition at line 84 of file common/ead_core/sl_bt_ead_core.h

mic#

sl_bt_ead_mic_t* sl_bt_ead_ad_structure_s::mic

Definition at line 85 of file common/ead_core/sl_bt_ead_core.h