Data structure of the data_length event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_connection_data_length_s::connection
Connection handle
Definition at line
6776
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
tx_data_len#
uint16_t sl_bt_evt_connection_data_length_s::tx_data_len
The maximum payload octets of a packet that the local Controller will send
Definition at line
6777
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
tx_time_us#
uint16_t sl_bt_evt_connection_data_length_s::tx_time_us
The maximum time in microseconds that the local Controller will take to send a data packet
Definition at line
6779
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
rx_data_len#
uint16_t sl_bt_evt_connection_data_length_s::rx_data_len
The maximum payload octets of a packet that the local Controller expects to receive
Definition at line
6781
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
rx_time_us#
uint16_t sl_bt_evt_connection_data_length_s::rx_time_us
The maximum time in microseconds that the local Controller expects to take to receive a data packet
Definition at line
6783
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h