Data structure of the config_complete event.
Public Attributes#
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_cs_config_complete_s::connection
Connection handle
12196
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
config_id#
uint8_t sl_bt_evt_cs_config_complete_s::config_id
ABR configuration identifier.
Range: 0 to 3
12197
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
status#
uint16_t sl_bt_evt_cs_config_complete_s::status
SL_STATUS_OK if successful. Error code otherwise.
12200
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
config_state#
uint8_t sl_bt_evt_cs_config_complete_s::config_state
Enum sl_bt_cs_config_state_t. ABR configuration state Values:
sl_bt_cs_config_state_removed (0x0): The ABR device configuration is removed
sl_bt_cs_config_state_created (0x1): The ABR device configuration is created
12203
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
main_mode_type#
uint8_t sl_bt_evt_cs_config_complete_s::main_mode_type
Enum sl_bt_cs_mode_t. Main mode type. Values:
sl_bt_cs_mode_calibration (0x0): Frequency offset and timing calibration measurement
sl_bt_cs_mode_rtt (0x1): Round Trip Time (RTT) measurement
sl_bt_cs_mode_pbr (0x2): Phase-Based Ranging (PBR) measurement
sl_bt_cs_mode_pbr_and_rtt (0x3): PBR and RTT measurement
12215
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
sub_mode_type#
uint8_t sl_bt_evt_cs_config_complete_s::sub_mode_type
Enum sl_bt_cs_mode_t. Sub mode type. Values:
sl_bt_cs_mode_calibration (0x0): Frequency offset and timing calibration measurement
sl_bt_cs_mode_rtt (0x1): Round Trip Time (RTT) measurement
sl_bt_cs_mode_pbr (0x2): Phase-Based Ranging (PBR) measurement
sl_bt_cs_mode_pbr_and_rtt (0x3): PBR and RTT measurement
12234
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
min_main_mode_steps#
uint8_t sl_bt_evt_cs_config_complete_s::min_main_mode_steps
Minimum number of ABR main mode steps to be executed prior to a sub mode step.
Range: 1 to 160
12253
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
max_main_mode_steps#
uint8_t sl_bt_evt_cs_config_complete_s::max_main_mode_steps
Maximum number of ABR main mode steps to be executed prior to a sub mode step.
Range: 1 to 160
12258
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
main_mode_repetition#
uint8_t sl_bt_evt_cs_config_complete_s::main_mode_repetition
Number of main mode steps taken from the end of the last ABR subevent to be repeated at the beginning of the current ABR subevent directly after the last Mode 0 step of that event.
Range: 0 to 3
12263
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
mode_calibration_steps#
uint8_t sl_bt_evt_cs_config_complete_s::mode_calibration_steps
Number of calibration mode steps to be included at the beginning of the test ABR subevent.
Range: 1 to 3
12272
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
role#
uint8_t sl_bt_evt_cs_config_complete_s::role
Enum sl_bt_cs_role_t. Device role during the ABR procedure Values:
sl_bt_cs_role_initiator (0x0): The device will initiate the procedure
sl_bt_cs_role_reflector (0x1): The device will reciprocate transmission
12277
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
rtt_type#
uint8_t sl_bt_evt_cs_config_complete_s::rtt_type
Enum sl_bt_cs_rtt_type_t. RTT payload type used in the ABR procedure Values:
sl_bt_cs_rtt_type_coarse (0x0): RTT Coarse
sl_bt_cs_rtt_type_fractional_96_bit_sounding (0x2): RTT Fractional with 96-bit Sounding Sequence
12289
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
cs_sync_phy#
uint8_t sl_bt_evt_cs_config_complete_s::cs_sync_phy
Enum sl_bt_gap_phy_t. Used PHY for ABR SYNC exchanges during a procedure Values:
sl_bt_gap_phy_1m (0x1): 1M PHY
12300
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
channel_map#
sl_bt_cs_channel_map_t sl_bt_evt_cs_config_complete_s::channel_map
A fixed length byte array of 10 bytes consisting of 79 1-bit fields.
The nth field (in the range 0 to 78) contains the value for the ABR channel index n.
Bit value 0: Channel n is disabled
Bit value 1: Channel n is enabled
The rest of most significant bits are reserved for future use and must be set to 0. Channels n = 0, 1, 23, 24, 25, 77 and 78 shall be ignored and not used for ABR. At least 15 channels shall be marked as used.
12307
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
channel_map_repetition#
uint8_t sl_bt_evt_cs_config_complete_s::channel_map_repetition
Number of times the channel_map field will be cycled through for non-Mode 0 steps within a ABR procedure.
Range: 0x01 to 0xFF
12331
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
channel_selection_type#
uint8_t sl_bt_evt_cs_config_complete_s::channel_selection_type
Enum sl_bt_cs_channel_selection_algorithm_t. ABR algorithm to be used during the procedure for non-mode 0 steps Value:
sl_bt_cs_channel_selection_algorithm_3b (0x0): Use Channel Selection Algorithm #3b for non-mode 0 ABR steps
sl_bt_cs_channel_selection_algorithm_3c (0x1): Use Channel Selection Algorithm #3c for non-mode 0 ABR steps
sl_bt_cs_channel_selection_algorithm_user_shape_interleaved (0x2): Use Interleaved shape for user specified channel sequence
12337
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
ch3c_shape#
uint8_t sl_bt_evt_cs_config_complete_s::ch3c_shape
Enum sl_bt_cs_ch3c_shape_t. Shape for user-specified channel sequence Values:
sl_bt_cs_ch3c_shape_hat (0x0): Use Hat shape for user specified channel sequence
sl_bt_cs_chc3_shape_interleaved (0x1): Use Interleaved shape for user specified channel sequence
12357
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
ch3c_jump#
uint8_t sl_bt_evt_cs_config_complete_s::ch3c_jump
Number of channels skipped in each rising and falling sequence
Range: 0x03 to 0x08
12371
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
companion_signal_enable#
uint8_t sl_bt_evt_cs_config_complete_s::companion_signal_enable
Enum sl_bt_cs_companion_signal_status_t. Enabled or disabled companion signal status Values:
sl_bt_cs_companion_signal_status_disable (0x0): The companion signal is disabled
sl_bt_cs_companion_signal_status_enable (0x1): The companion signal is enabled
12375
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h