Data structure of the descriptor event.

Public Attributes#

uint8_t
uint16_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_gatt_descriptor_s::connection

Connection handle


Definition at line 7687 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

descriptor#

uint16_t sl_bt_evt_gatt_descriptor_s::descriptor

GATT characteristic descriptor handle


Definition at line 7688 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

uuid#

uint8array sl_bt_evt_gatt_descriptor_s::uuid

Descriptor UUID in little endian format


Definition at line 7689 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h