Modules#
sl_bt_evt_gatt_server_characteristic_status_s
sl_bt_evt_gatt_server_characteristic_status#
Indicates either that a local Client Characteristic Configuration descriptor was changed by the remote GATT client, or that a confirmation from the remote GATT client was received upon a successful reception of the indication.
A confirmation by the remote GATT client should be received within 30 seconds after an indication was sent with the sl_bt_gatt_server_send_indication command, otherwise further GATT transactions over this connection are not allowed by the stack.
Typedefs#
Macros#
#define
Identifier of the characteristic_status event.