Connection TX status flags#
Defines the connection TX status flags reported by sl_bt_resource_get_connection_tx_status.
Macros#
The number of TX packets queued on a connection has overflowed the packet_count that was effective at the time the connection opened. The packet count is configured with command sl_bt_resource_enable_connection_tx_report and is valid for subsequent connections.
When this bit is set, the packet_count returned by sl_bt_resource_get_connection_tx_status is correct, but data_len excludes the data bytes in the packets that overflowed the configured packet count.
Internal inconsistency has been detected in the connection TX bookkeeping. When this bit is set, the application should consider both packet_count and data_len returned by sl_bt_resource_get_connection_tx_status to be unreliable.
Macro Definition Documentation#
SL_BT_RESOURCE_CONNECTION_TX_FLAGS_ERROR_PACKET_OVERFLOW#
#define SL_BT_RESOURCE_CONNECTION_TX_FLAGS_ERROR_PACKET_OVERFLOWValue:
0x1
The number of TX packets queued on a connection has overflowed the packet_count that was effective at the time the connection opened. The packet count is configured with command sl_bt_resource_enable_connection_tx_report and is valid for subsequent connections.
When this bit is set, the packet_count returned by sl_bt_resource_get_connection_tx_status is correct, but data_len excludes the data bytes in the packets that overflowed the configured packet count.
SL_BT_RESOURCE_CONNECTION_TX_FLAGS_ERROR_CORRUPT#
#define SL_BT_RESOURCE_CONNECTION_TX_FLAGS_ERROR_CORRUPTValue:
0x2
Internal inconsistency has been detected in the connection TX bookkeeping. When this bit is set, the application should consider both packet_count and data_len returned by sl_bt_resource_get_connection_tx_status to be unreliable.