Modules#

sl_bt_evt_connection_remote_tx_power_s

sl_bt_evt_connection_remote_tx_power#

Reports a transmit power change of the connection on the remote device that supports the LE Power Control for the connection.

This event is enabled if reporting the remote transmit power change has been enabled with the sl_bt_connection_set_remote_power_reporting command.

Macros#

#define

Identifier of the remote_tx_power event.

Typedef Documentation#

sl_bt_evt_connection_remote_tx_power_t#

typedef struct sl_bt_evt_connection_remote_tx_power_s sl_bt_evt_connection_remote_tx_power_t

Macro Definition Documentation#

sl_bt_evt_connection_remote_tx_power_id#

#define sl_bt_evt_connection_remote_tx_power_id
Value:
0x070600a0

Identifier of the remote_tx_power event.