Data structure of the data event.

Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_external_bondingdb_data_s::connection

Connection handle


Definition at line 11351 of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

type#

uint8_t sl_bt_evt_external_bondingdb_data_s::type

Enum sl_bt_external_bondingdb_data_t. The bonding data type. Values:

  • sl_bt_external_bondingdb_data_remote_address (0x0): Identity address of the remote device, which a resolvable random address can be resolved to

  • sl_bt_external_bondingdb_data_remote_address_type (0x1): Type of the remote device identity address. Value 0 is public device address and 1 is static device address

  • sl_bt_external_bondingdb_data_remote_ltk (0x2): Long Term Key (LTK) used as central device. The value of this type must be stored securely.

  • sl_bt_external_bondingdb_data_local_ltk (0x3): Long Term Key (LTK) used as peripheral device. The value of this type must be stored securely.

  • sl_bt_external_bondingdb_data_remote_central_inf (0x4): Identification info used as a central device

  • sl_bt_external_bondingdb_data_local_central_inf (0x5): Identification info used as a central device

  • sl_bt_external_bondingdb_data_irk (0x6): Identity Resolving Key (IRK) of the remote device that is used for resolving its RPA addresses when the device is in privacy mode. The value of this type must be stored securely.

  • sl_bt_external_bondingdb_data_meta (0x7): Metadata about the bonding

  • sl_bt_external_bondingdb_data_gatt_client_config (0x8): The remote GATT client characteristic configurations

  • sl_bt_external_bondingdb_data_gatt_client_features (0x9): The remote GATT client supported features

  • sl_bt_external_bondingdb_data_gatt_db_hash (0xa): Latest local GATT database hash value that the remote client has seen for GATT robust caching feature


Definition at line 11352 of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

data#

uint8array sl_bt_evt_external_bondingdb_data_s::data

Bonding data


Definition at line 11394 of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h