Data structure of the subevent_tx_failed event.
Public Attribute Documentation#
advertising_set#
uint8_t sl_bt_evt_pawr_advertiser_subevent_tx_failed_s::advertising_set
The PAwR advertising set handle for the PAwR train that failed to transmit subevent data
Definition at line
5993
of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
subevent#
uint8_t sl_bt_evt_pawr_advertiser_subevent_tx_failed_s::subevent
The subevent that failed to transmit subevent data
Definition at line
5995
of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h