Modules#
sl_bt_evt_system_boot_s
sl_bt_evt_system_boot#
Indicates that the device has started and the radio is ready.
This event carries the firmware build number and other software and hardware identification codes.
Macros#
#define
Identifier of the boot event.
Typedef Documentation#
sl_bt_evt_system_boot_t#
typedef struct sl_bt_evt_system_boot_s sl_bt_evt_system_boot_t
Definition at line 781
of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_system_boot_id#
#define sl_bt_evt_system_boot_id
Value:0x000100a0
Identifier of the boot event.
Definition at line 763
of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h