Data structure of the rssi event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_connection_rssi_s::connection
Connection handle
Definition at line
7060
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
status#
uint8_t sl_bt_evt_connection_rssi_s::status
Command complete status which is always SL_STATUS_OK
Definition at line
7061
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
rssi#
int8_t sl_bt_evt_connection_rssi_s::rssi
The median of the last seven measured RSSI values on the connection. Units: dBm. Range: -127 to +20.
Definition at line
7062
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h