Data structure of the characteristic event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_gatt_characteristic_s::connection
Connection handle
Definition at line
8060
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
characteristic#
uint16_t sl_bt_evt_gatt_characteristic_s::characteristic
GATT characteristic handle
Definition at line
8061
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
properties#
uint8_t sl_bt_evt_gatt_characteristic_s::properties
Characteristic properties
Definition at line
8062
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
uuid#
uint8array sl_bt_evt_gatt_characteristic_s::uuid
Characteristic UUID in little endian format
Definition at line
8063
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h