sl_bt_evt_advertiser_timeout#

Indicates the legacy or extended advertising on an advertising set has stopped because the advertiser has completed the configured number of advertising events or the advertising has reached the configured duration.

The maximum number of advertising events or advertising duration can be configured by the maxevents or duration parameter in the command sl_bt_advertiser_set_timing.

Modules#

sl_bt_evt_advertiser_timeout_s

Macros#

#define

Identifier of the timeout event.

Typedef Documentation#

sl_bt_evt_advertiser_timeout_t#

typedef struct sl_bt_evt_advertiser_timeout_s sl_bt_evt_advertiser_timeout_t

Definition at line 2130 of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_advertiser_timeout_id#

#define sl_bt_evt_advertiser_timeout_id
Value:
0x010400a0

Identifier of the timeout event.


Definition at line 2120 of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h