Data structure of the report event.

Public Attributes#

uint8_t

Public Attribute Documentation#

analyzer#

uint8_t sl_bt_evt_connection_analyzer_report_s::analyzer

The handle of the connection analyzer


central_rssi#

int8_t sl_bt_evt_connection_analyzer_report_s::central_rssi

RSSI measurement of the packet transmitted by the Central device. Units: dBm. Range: -127 to +20.


peripheral_rssi#

int8_t sl_bt_evt_connection_analyzer_report_s::peripheral_rssi

RSSI measurement of the packet transmitted by the Peripheral device. Units: dBm. Range: -127 to +20.