Data structure of the subevent_data_request event.
Public Attribute Documentation#
advertising_set#
uint8_t sl_bt_evt_pawr_advertiser_subevent_data_request_s::advertising_set
The PAwR advertising set handle
Definition at line
6060
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
subevent_start#
uint8_t sl_bt_evt_pawr_advertiser_subevent_data_request_s::subevent_start
The first subevent that data is requested for
Definition at line
6061
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
subevent_data_count#
uint8_t sl_bt_evt_pawr_advertiser_subevent_data_request_s::subevent_data_count
The number of subevents that data is requested for
Definition at line
6063
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h