sl_bt_evt_system_awake#

Indicates that the device is awake and no longer in sleep mode.

NOTE: Stack does not generate this event by itself because sleep and wakeup are managed by applications. If this event is needed, call function sl_bt_send_system_awake, which signals the stack to send the event.

Macros#

#define

Identifier of the awake event.

Macro Definition Documentation#

sl_bt_evt_system_awake_id#

#define sl_bt_evt_system_awake_id
Value:
0x040100a0

Identifier of the awake event.


Definition at line 954 of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h