Data structure of the phy_status event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_connection_phy_status_s::connection
Connection handle
Definition at line
6659
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
phy#
uint8_t sl_bt_evt_connection_phy_status_s::phy
Current active PHY. See values from sl_bt_connection_set_preferred_phy command.
Definition at line
6660
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h