Data structure of the boot event.

Public Attributes#

uint16_t
uint16_t
uint16_t
uint16_t
uint32_t
uint16_t
uint32_t

Public Attribute Documentation#

major#

uint16_t sl_bt_evt_system_boot_s::major

Major release version


Definition at line 784 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

minor#

uint16_t sl_bt_evt_system_boot_s::minor

Minor release version


Definition at line 785 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

patch#

uint16_t sl_bt_evt_system_boot_s::patch

Patch release number


Definition at line 786 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

build#

uint16_t sl_bt_evt_system_boot_s::build

Build number


Definition at line 787 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

bootloader#

uint32_t sl_bt_evt_system_boot_s::bootloader

Unused. Ignore this field.


Definition at line 788 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

hw#

uint16_t sl_bt_evt_system_boot_s::hw

Hardware type: the major chip revision number in the most significant byte and the minor revision in the least significant byte


Definition at line 789 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

hash#

uint32_t sl_bt_evt_system_boot_s::hash

Version hash


Definition at line 792 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h