Hall Effect GATT Service#
Provides hall sensor data in GATT characteristics. Designed for the Thunderboard smartphone app.
Functions#
void
sl_gatt_service_hall_on_event(sl_bt_msg_t *evt)
sl_status_t
sl_gatt_service_hall_get(float *field_strength, bool *alert, bool *tamper)
Macros#
#define
SL_GATT_SERVICE_HALL_FIELD_STRENGTH_INVALID 0x7FFFFFFF
#define
SL_GATT_SERVICE_HALL_ALERT_INVALID false
#define
SL_GATT_SERVICE_HALL_TAMPER_INVALID true
Function Documentation#
sl_gatt_service_hall_on_event#
void sl_gatt_service_hall_on_event (sl_bt_msg_t * evt)
Parameters
[in] | evt | Event coming from the Bluetooth stack. |
Bluetooth stack event handler.
Definition at line
45
of file common/gatt_service_hall/sl_gatt_service_hall.h
sl_gatt_service_hall_get#
sl_status_t sl_gatt_service_hall_get (float * field_strength, bool * alert, bool * tamper)
Parameters
[out] | field_strength | Field strength level (in mT). |
[out] | alert | Field strength has reached the alert level. |
[out] | tamper | Field strength has reached the tamper level. |
Getter for Field Strength and State characteristic values. Returns
Status of the operation.
Note
To be implemented in user code.
Definition at line
55
of file common/gatt_service_hall/sl_gatt_service_hall.h