Environment Sensing - Air Pressure GATT Service#
Provides air pressure sensor data in GATT characteristics. Designed for the Thunderboard smartphone app.
Functions#
void
sl_gatt_service_pressure_on_event(sl_bt_msg_t *evt)
sl_status_t
sl_gatt_service_pressure_get(float *pressure)
Macros#
#define
SL_GATT_SERVICE_PRESSURE_INVALID 0xFFFFFFFF
Function Documentation#
sl_gatt_service_pressure_on_event#
void sl_gatt_service_pressure_on_event (sl_bt_msg_t * evt)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_bt_msg_t * | [in] | evt | Event coming from the Bluetooth stack.  | 
Bluetooth stack event handler.
sl_gatt_service_pressure_get#
sl_status_t sl_gatt_service_pressure_get (float * pressure)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| float * | [out] | pressure | Barometric pressure (in millibars).  | 
Getter for Pressure characteristic value. Returns
Status of the operation.
Note
To be implemented in user code.