sl_bt_evt_advertiser_scan_request#
Reports a scan request received during the legacy or extended advertising advertising if the scan request notification is enabled.
Modules#
sl_bt_evt_advertiser_scan_request_s
Typedefs#
Macros#
#define
sl_bt_evt_advertiser_scan_request_id 0x020400a0
Identifier of the scan_request event.
Typedef Documentation#
sl_bt_evt_advertiser_scan_request_t#
typedef struct sl_bt_evt_advertiser_scan_request_s sl_bt_evt_advertiser_scan_request_t
Definition at line
2083
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_advertiser_scan_request_id#
#define sl_bt_evt_advertiser_scan_request_idValue:
0x020400a0
Identifier of the scan_request event.
Definition at line
2036
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h