Data structure of the rssi event.

Public Attributes#

uint8_t
uint8_t
int8_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_connection_rssi_s::connection

Connection handle


Definition at line 6066 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

status#

uint8_t sl_bt_evt_connection_rssi_s::status

Command complete status which is always SL_STATUS_OK


Definition at line 6067 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

rssi#

int8_t sl_bt_evt_connection_rssi_s::rssi

The median of the last seven measured RSSI values on the connection. Units: dBm.


Definition at line 6068 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h